FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
12-12-2023 02:22 PM - edited 12-12-2023 02:30 PM
Hello everyone, I encountered the following issue:
Used software :
After enabling the proxy tool (Px.exe) and configuring the proxy settings (ctrlX Core Virtual -> Settings -> Proxy) NodeRED web app displays the message: The app is currently not available. I waited for 10+ minutes, refreshed the page but I got the same message.
However, when I disable the proxy settings (ctrlX Core Virtual -> Settings -> Proxy). NodeRed starts flawlessly. However, since I am connected to a corporate WiFi network, I do not have any internet access in the ctrlX Core.
Note: I managed to resolve the issue by downgrading to a lower version of the:
Solved! Go to Solution.
12-13-2023 03:31 PM - edited 12-13-2023 03:37 PM
Hello,
See, we were able to reproduce, we will open an internal ticket to fix this 🙂
PS i tried with the image 2.04 and node-red 2.2.0+3.0.2-ctrlx and is also working! so i think we have to check what is new in node-red from this point of view 🙂
12-18-2023 09:32 AM
did u check also with 2.4 image and node-red version 2.2.0+3.0.2-ctrlx. FOr me is working, can you check on your setup please? 😁
12-18-2023 01:16 PM - edited 12-18-2023 01:16 PM
Hi,
sorry for the late reply. I just tested your mentioned configuration 2.4 image and node-red version 2.2.0+3.0.2-ctrlx and I can confirm that NodeRED starts sucessfuly. 🙂
12-27-2023 11:16 AM
We are working on a more clean way to start node-red with the proxy for the next releases 😁
meanwhile i don't think that makes really a huge difference to use this or the other version!
12-28-2023 09:16 AM
Got it, thanks for the update! Closing the ticket now. 🙂
06-14-2024 11:00 PM
Where did you download that NodeRED version of the app "node-red version 2.2.0+3.0.2-ctrlx"? I only found the "Node-RED 2.4.0+3.1.0-ctrlx" with the image "2.4.0" from collaboration rooms. The CtrlX can connect to the Internet as the proxy is already running, but cannot start NodeRED app...
06-17-2024 08:01 AM
@cal9mx2 please check out latest version "Node RED RED-V-0206.2+3.1.7-ctrlx"
@MauroRiboniMX did you test the latest version already?
06-17-2024 09:39 AM
Affermative 😊. Should be solved from 2.6 this issue
07-22-2024 05:55 AM
Hi,
Same issue happening to ctrlX virtual base image version 1.20.13 with node-red. And my ctrlX works not able to get the older version image. How to resolve this?
07-22-2024 08:11 AM
Hello,
Which node-red version? 😀. I give a look today again
07-23-2024 04:26 AM
Hi im using this version,
Node RED RED-V-0120.2+3.0.2
07-23-2024 04:49 PM - edited 07-23-2024 04:49 PM
Should be solved in the next release with 2.60 release, end of this month
07-24-2024 02:55 AM
But i am using image version 1.20.13. it cannot use version 2 apps right?
07-24-2024 08:41 AM
Hello,
No but technically should be fixed in the nex version, i have to check with developers. I think you are doing a connection for PX proxy right?
This setting is solving the issue 😁. Meanwhile we check with the devs when the fix is coming
07-24-2024 09:36 AM
just a question, can't you find the older apps version in the collab room?
07-24-2024 03:48 PM
I'm finding a limited number of images and app versions on both the US and DE collaboration rooms. Usually only 1 patch per major release.
07-24-2024 04:15 PM
next release will be 1.20.9 for node-red and will solve that. by that time i suggest you to use the "workaround" or either move to 2.6.x Globally the fix for this problem is integrated in version: 1.20.9, 2.6.5, 3.2.0.
07-24-2024 04:19 PM
Regarding this, we are not allowed to ship the older versions, for security reasons. Checked now.
if there is for example a vulnerability, we have to patch it and we are not allowed to ship the vulnerable version anymore.
This is the law.
07-25-2024 09:55 AM
Hi, by doing so does it mean my Virtual Control Cannot access to the internet? because i still not able to install pallete.
07-25-2024 01:36 PM
Yes,
That is the bug happening with the workaroung. When you do that settings that is no more working. with 1.20.9 will be fixed
08-06-2024 04:50 AM
Where did you download the NodeRED version "NodeRED RED-V-120.0+3.0.2-ctrlx"?
Did that fix the issue? I currently have a Virtual Core 1.20.12 (image version), that is imitating the issue of a physical core, that cannot be upgraded.
On the store only found version 3.1.
08-06-2024 05:03 AM
@CodeShepherd and @MauroRiboniMX I already tried with the newest versions and I can connect to the internet, but cannot download any plugins from the pallet manager in NodeRed.
Here is my CtrlX Virtual version (2.6.8 image version) & my NodeRed Version (NodeRED 2.6.5+3.1.11-ctrlx).
I leave here my newest post with more details if you can help me: NodeRED - Cannot install plugins via NodeRed Pallete Manager (InfluxDB plugin error) (boschrexroth.c...
a month ago
Hello,
Can you send here the proxy page configuration?