04-17-2023 05:25 PM
I installed the latest pre-release versions of these apps but when I try to open them I get the following error. I tried to update the system apps but the situation is still the same.
Solved! Go to Solution.
04-17-2023 10:07 PM
For IoT Dashboard V1.20 and InfluxDB App V1.20 its prerequisite to have the System Apps V1.20. Maybe there is an issue with first installing the Application Apps and afterwards updating the Sytem Apps.
I would recommend to uninstall and reinstall the InfluxDB and IoT Dashboard Apps.
Best regards,
Nick
04-19-2023 10:29 AM
Thanks for the reply!
After a firmware and kernel update, I reinstalled the apps and they all work fine now. Also I fixed an issue with placeholder callables in the scheduler that was provably causing the ctrlx to not work properly.
Kind regards,
Berk