07-06-2023 11:09 AM
Hello,
I need to swap hardware. I just want to save a backup of the old CtrlX3 and load it onto the new CtrlX7.
Unfortunately, this procedure does not work. When restoring, an error is always displayed. I have attached a picture of the error message.
How is the procedure planned to replace the hardware?
Solved! Go to Solution.
07-06-2023 11:36 AM
What version are you using? Backup and restore is not for switching from one control to an other.
Depending of the version you are using there is a possibility by using the setup functionality.
Or you can just save the configuration and upload it to the X7.
07-06-2023 12:03 PM
07-06-2023 01:17 PM
Hello, to use X7 i recommend to update ctrlX Works to 1.20
The versions of the apps you can find either from HOME --> + install an app or via Settings --> APPs
Or you can generate a system report and attach it here, than i can read out the version.
And here you even can find the online-help.
If you have still problems we can do a teams-call too.