cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Ethercat Bus cannot exceed 2000us

Ethercat Bus cannot exceed 2000us

aFouraker
Occasional Contributor

When I try and take the ethercat bus to 4ms instead of the default 2ms I get the error that I cannot exceed 2ms. My application does not need 2ms and this is taxing the processor unneccesarily. Is there a way to have a higher cycle time for Ethercat?

2 REPLIES 2

CodeShepherd
Community Moderator
Community Moderator

At the moment the EtherCat fieldbus cycle time is fixed to 2ms. We are working on this to bring it up mid or end of this year.

The EtherCat itself does not produce high load to the CPU. This only happens if other application s like big PLC programs or own apps are directly bound to it.

This feature (to change the EtherCAT cycle time to 4 ms) is planned for RM22.07 (V1.16).

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist