cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

WebIQ Designer only 30 tags after license of 150tags activated

WebIQ Designer only 30 tags after license of 150tags activated

AndroidzZ
New Contributor

I just upgraded my ctrlX to Ubuntu 20. And i installed core18 parrelel to the system app core20 to maken WebIQ work.

Now I just installed the 150 tags Licenese for WebIQ but my webiq Designer still says I can only use a limit of 30 variables? See pic.

IS this because of the upgrade to ubuntu20 or is there something else at play? 

 

3 REPLIES 3

I did look at the topic. I deleted and reinstalled the WebIQ runtime app while the license was activated.

But I still have a free edition WebIQ Designer with only 30 tags.

Any other ideas? 

After reinstalling webiq runtime app I started WebIQ designer from my local stored designer, see: 

AndroidzZ_0-1649236074179.png

But it seems to be that I have to start-up my designer throught de CORE with the following command to makeuse of the license, see: 

AndroidzZ_1-1649236213022.png

 

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist