Tips to use localization in WebIQ

Tips to use localization in WebIQ

HmiGuide
Community Moderator
Community Moderator
How can I change the default language?
How can I use the export file?

 

2 REPLIES 2

HmiGuide
Community Moderator
Community Moderator
How can I change the default language?

The only way to do this in WebIQ 1.10 is changing a json file.

  • Publish your project, to have a backup, if anything fails
  • Edit file: %AppData%\webiq-designer\workspace\json\local\index.json
  • Replace item “default” language (marked blue) with any of the other languages (marked red)
{
    "default": "de-DE",   
    "locales": {
        "de-DE": {
            "label": "Deutsch",
            "region": "DE",
            "keyboard": "de"
        },
        "en-GB": {
            "label": "English",
            "region": "GB",
            "keyboard": "us"
        }
    },
    // end of file not shown here
  • Save file
  • Close “Localization Manager” to enable update
  • Open it again. Verify that the default language changed.
How can I use the export file?

Question:

I added a new language and exported it. The file (csv and json) only contains the localization variables, but I need the texts of my default language to be able to translate it.

Workaround:

In WebIQ 1.10 there is no way to create a export file with multiple languages. But you can do it by yourself.

  • Export a csv file with the 1st language (containing your texts)
  • Export a csv file with the 2nd language (which should be translated)
  • Open both files in Excel
  • Copy content of 1st file into 2nd file into columns D+E (the order of the keywords is identical)
  • Translate everything
  • Remove all columns except A + B
  • Save csv file
  • Import csv file into WebIQ
  • Use Excel function =IF(A1=D1;” ”;”x”)to verify if varNames are identical

StefBaro_0-1635328601569.png

 

webiq-eg
Long-established Member

Hi,
also this ticket is old: In WebIQ 2.12 the default language can be set in the Localisation Manager:

webiqeg_1-1663239343876.png

Choose a language that is not the default language. Then you can make it the default language via the Settings menu.
Have fun with WebIQ.
webiq-eg

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist