09-21-2023 10:28 AM
Hello Together,
I am facing an issue in my Project on updating a Custom Widget. The error shows the dependeny to already uninstalled custom widget. I did not want to redo my project in order to eleminate this dependeny therefore would like to more about this. As per my understanding this error starts to show after i updated my WebIQ designer from V2.13 -> V2.14.
Solved! Go to Solution.
09-21-2023 04:08 PM
The error in the console shows an error in your custom widget's LESS code that need to be fixed. These were previously not shown, but were still there. They are shown since 2.14 (WEBIQ-3722, see https://www.smart-hmi.com/user/download/deliver/docs/documentation-webiq-changelog-master-7792/index...)
The errors in Package Manager indicate that the files from your custom widgets are already included in the HMI, but the HMIs meta information does not record that you installed them. This might happen if you e.g. install the widgets and commit the changes in your VCS like GIT without committing all files of the HMI and then checking out the HMI on a different system with the updated meta information missing.
If you want us to look into this please provide the HMI - you can also send it via PM.