Monday
Hello everyone. This code below works on the computer view of WebIQ (Google Chrome Web Browser for Windows 11), but this code does not work on the tablet view of WebIQ (Google Chrome Android app).
The code of WebIQ v2.15.4, Javascript:
Tuesday
Your JavaScript code does not relate to WebIQ widgets, but is pure JavaScript to obtain an HTMLElement from the DOM and track clicks. As you're using WebIQ you should use the framework's functions for this instead as widgets are more complex than basic HTML elements.
As you did not specify what you actually want to achieve I can only try to deduct from what you wrote - I assume you want to reload the HMI on click on a WebIQ Button widget. In this case you should always not write custom code to get the button somehow, but simply create a custom UI Action to perform the action.
You only have to write code to get widget instances if you want to track the clicks from a LocalScript instead - but that wouldn't make sense if you only want to track button clicks in general - it's just a one-liner - create a custom UI Action in Code Manager and add the line "location.reload();":
Then simply add your custom UI Action to the button widget you wish to execute the action on and you're done.
If this is not what you want to achieve please explain what you want to achieve.
Please note that the Scripting Demo contains some very well documented code if you want to do this from a LocalScript instead (which for a normal use case would not be recommended in this case): https://demo.smart-hmi.com/scripting-demo/js/custom-libs/local-scripts/demo-dynamic-widgets.js
Tuesday - last edited Tuesday
I found the solution to this problem today.
Problem was: Working buttonOnClick method was not working on the tablet screen because of different performAction handling required.
Solution approach: I tried all of the methods in this code block below:
Tuesday
This is not the intended way to use it and not guaranteed to work in the future. When using a framework like Angular, React, Vue.js or, incidentally, WebIQ Visuals you should always use the framework methods, not Vanilla JS when it comes to handling interactivity.
Wednesday
As a summary: when using WebIQ's built-in functionality it handles all of those things like touchstart and touchend correctly. This is not a WebIQ issue.