Hello,
inside the package.manifest.json file I have some scopes defined. This scopes are assigned to permissions inside the "menu" struct.
But the items on the ctrlX main menu can be called by any user, even if they do not have the necessary permissions.
The user have the correct permissions assigned and also the JWT permissions are correct.
How can I restrict the access of items inside the ctrlx menu, sidebar and settings?
Thanks!
Solved! Go to Solution.
Hello
Currently it is not possible to restrict the access of the ctrlX sidebar over the User&Permissions.
Means you can open every page linked in the ctrlX menue. If you don’t have the permission you will get a message that you are not allowed to use the function of this page. (unfortunately at some pages cryptical)
I will make a requirement of the (useful) feature into the develepment pipeline...
Regards
Jochen
Hi,
Thanks for the answer. Can I get feedback on when the feature is available?
Thank you!
Regards
Wolfgang
The feature is now in the development backlog.
No sheduling until now. Sorry.
Are there any updates on this topic?
Update 07.06.2022
currently no change of the situation.
no date for realization, because of limited development resource. The feature is still in the development backlog for 2022. Priority is now increased. So hopeful we have ist latest end of this year. (no guaranty...)
Regards
Jochen Müller