Communication Size Limits

Communication Size Limits

DCEN_Tony
Established Member

Hello

I have been asked to find out what Input/output byte size limitations the various Ethernet based commuications possibilities are with a CtrlX Core in Drive: 

1. CtrlX OS  Profinet Device - Max number of  Input/ output bytes that can be declared?

2. CtrlX OS OPC UA Pub/Sub and Client - Any restriction on number of read/write data bytes in one packet?

3. CtrlX OS OPC UA Server - Any restriction on data table size?

4. CODESYS Ethernet IP Adapter - Max number of  Input/ output bytes that can be declared?

5. CODESYS Profinet Device - Max number of  Input/ output bytes that can be declared?

6. CODESYS TCP/UDP Function blocks - Max packet size?

7. CODESYS MQTT - Max packet size?  ( I have seen Solved: adjust Maximun packet size in the parameter list (boschrexroth.com) but it wasn't clear if there was any restriction)

I have done various offline tests (e.g. 4 and 5 above did not seem to generate any errors with huge IO size) and searched documentation but struggling to find definitive answers....maybe it is just a limit of network and hardware performance?

Many Thanks

2 REPLIES 2

Thoomas
Community Moderator
Community Moderator

I start with some answers – links into the documentations:

  1. CtrlX OS  Profinet Device - Max number of  Input/ output bytes that can be declared?
    EN: https://docs.automation.boschrexroth.com/doc/3703895296/profinet-device-app-features/latest/en/?sel=...
    DE: https://docs.automation.boschrexroth.com/doc/3703895296/profinet-device-app-features/latest/de/?sel=...
  2. CtrlX OS OPC UA Pub/Sub and Client - Any restriction on number of read/write data bytes in one packet?
    For clients see the links below and the links for the OPC UA Server:
    EN: https://docs.automation.boschrexroth.com/doc/894340029/eigenschaften/latest/en/?sel=AwegjCAsKq0EwC5g...
    DE: https://docs.automation.boschrexroth.com/doc/894340029/eigenschaften/latest/de/?sel=AwegjCAsKq0EwC5g...
  3. CtrlX OS OPC UA Server - Any restriction on data table size?
    EN: https://docs.automation.boschrexroth.com/doc/412150158/eigenschaften/latest/en/?sel=AwegjCAsKq0EwC5g...
    DE: https://docs.automation.boschrexroth.com/doc/412150158/eigenschaften/latest/de/?sel=AwegjCAsKq0EwC5g...

For all CODESYS fieldbus communications see the link below and the linked sites by CODESYS directly:
CODESYS - Fieldbus Communication (boschrexroth.com)

  1. CODESYS Ethernet IP Adapter - Max number of  Input/ output bytes that can be declared?
  2. CODESYS Profinet Device - Max number of  Input/ output bytes that can be declared?
  3. CODESYS TCP/UDP Function blocks - Max packet size?
  4. CODESYS MQTT - Max packet size?  ( I have seen Solved: adjust Maximun packet size in the parameter list (boschrexroth.com) but it wasn't clear if there was any restriction)

Hi,

point 6, I tried it and got a max number of 65507 Bytes for UDP.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist