cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Add parameters to ProfiNet data confuguration

Add parameters to ProfiNet data confuguration

Mike_T
Member

Hello,

Below in Slot 1 of the master communication we have a problem adding parameters to the data configuration.

When the '+' button to app a parameter is pressed, nothing hapens, no parameter will be added.

2022-07-06_11h47_16.png

 

The only possibility is to load a parameterfile including a parameter for the data configuration at first.

Then the data configuration can be extended only by the '+' button behind an existing parameter, like below.

Mike_T_0-1657107173316.png

 

Firmware used:

Mike_T_1-1657109258360.png

 

Is this a known issue and is there a solution?

 

Greetings, Mike

 

 

 

2 REPLIES 2

CodeShepherd
Community Moderator
Community Moderator

It is a known bug that as long as there are no parameter in the list the add button does not work. Can you tell us which version of ctrlX IO Engineering you are using?

Instead of loading a parameter file you could use the parameter editor to directly change the underlying list parameters P-0-4080 and P-0-4081.

We will have to check when it will be fixed.

Any news here or can this topic be closed?

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist