09-19-2022 02:17 PM
Hello,
A customer is using the XML_Utility_SL library to convert some data to XML. He is using the FB XMLFindElement and XMLWrite.
It works fine until it gives an error. Then he could not restart FB and needs to do a Clear all or reboot the CtrlX to get FB working again.
I attach pictures. In the picture it seems that the error is Invalid_License.
Any idea why this is happening?
Thanks in advance.
Solved! Go to Solution.
01-16-2023 08:09 AM
Is this still an issue or can this topic be closed?
01-16-2023 08:46 AM
Hello CodeShepherd,
I have no feedback from the customer, so I understand that he has solved it himself.
You can close the issue.
Thanks.