FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
02-02-2023 12:18 PM
Good Day,
I am trying to connect an S20 ProfiNet bus coupler to the CtrlX core X3 via the Codesys ProfiNet package I installed. I have followed the instructions in the manual that comes with the Codesys package, but am unable to install the device into my project. When I scan for devices it is picked up and then I set the name and IP address (which is accepted), but I keep getting an RPC Aborted error.
Is there anyone that could possibly assist me? I am sure I am doing something wrong or missing some other files possibly.
Thanks in advance.
Solved! Go to Solution.
02-11-2023 07:33 PM
personal message to setup a meeting follows.
02-14-2023 09:44 AM
Hello,
here to finish the request - quick sum up.
After the include of the corresponding CodesysPackage via the Codesys PackageManager the Ethernet-port was addable.
Configuring to PNController and leaving the default setting made the scan of the device work. Unfortunatley/gladely I struggled by using the misfitting gsdml- PN device description. the database had a version of S20-PN-BK which was misfitting to my S20-PN-BK+
The PRC status message guided to by saying "unkown device connected" .
Solution: update repository with correct gsdml file and try again.
Bye
02-15-2023 07:17 AM
apologies for the late reply, I was out of town. Thank you for your assistance I got it working,
Regards,