FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
10-13-2021 12:03 PM
Re: ctrlX CODESYS SoftMotion Adaption 1.10.0.3
I am able to successfully write to 4-byte drive parameters using SMC3_ETC_SoE_IdnWrite4:
However, SMC3_ETC_SoE_IdnRead4 configured similarly fails to return data:
Note that the FB completes execution (xDone=TRUE) but that uisDataLength is wrong (2, not 4).
Does anyone have any input on this?
Library version CXA_ETC_ITF (Bosch Rexroth) is 4.10.0.0.
Solved! Go to Solution.
10-14-2021 12:11 PM
I think this is related to the CXA_ETC_ITF (Bosch Rexroth) is 4.10.0.0 need to be debugged in there, only a guess
10-25-2021 05:45 PM - edited 10-25-2021 05:46 PM
The Problem (Bug 389272) will be resolved with ctrlX CORE 01V12 (release milestone RM 21.11).