cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Write to data layer stopps after few seconds

Write to data layer stopps after few seconds

E_Stapel
Long-established Member

Hello everyone,

i want to see my data on the data layer via the devicebridge. I created my Device (Driver Modbus TCP), the connector (Ctrlx DataLayer Connector) and the Collector (JSON Collector). When I start the collector, everything works and I can see the realtime data on the Data Layer. The Problem is, that I can see the data only for a few seconds and than the Layer "devicebridge" disappears. Going back to the collector I can see, that he is automatically turned off. 

How can I ensure, that the Collector always stays on, to have the data at all times on the data layer?

Thanks in advance. 

2 REPLIES 2

DvB_Support
Long-established Member

Hello E_Stapel,

I assume the collector was run in debug mode by clicking the green coloured run icon within the collector screen.

I kindly request to deploy the use case for seamless data stream to data layer by doing below steps in sequence,

  • 1. Click on Routing -> Add a route -> Choose the collector and data layer connector, Link it. (Routing image attached)
  • 2. Click on Service Container -> Drag & Drop the route created, Save it. (Route_Inside_ServiceContainer image attached)
  • 3. Publish -> Deploy / Publish the usecase provided all the checks are green (Publish_the_Usecase image attached)
  • 4. Service Monitoring -> Deployed service should be in running state as shown in the attachment (DeployedService image attached)
  • 5. Data streaming video attached too

Hope this clarifies

Thanks

Product Support

 

E_Stapel
Long-established Member

Hello @DvB_Support ,

thank you so much!

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist